Ultrasonic Sensors FAQ

Quality/Reliability
Waterproof type/Open-Structure type/High-Frequency type

Can Murata ultrasonic sensors be used under water?

Murata ultrasonic sensors are designed for use in the air and not under water.
The open structure and high-frequency types should not be used outdoors, either.
They cannot be used in environments where they are exposed to rain and/or dust.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send