Ultrasonic Sensors FAQ

Quality/Reliability
Waterproof type/Open-Structure type/High-Frequency type

Do Murata ultrasonic sensors cause health problems?
Do ultrasonic waves affect the health of the human body or animals (pets)? 

There are no laws that regulate the “sound volume” of aerial ultrasonic waves. As a general guideline, it is reported that long exposure to ultrasounds of 105-115dB or more may cause buzzing in the ear and discomfort. It is recommended that the ultrasonic volume be kept below the above limit in the sensor range used.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send