Small Energy Devices FAQ

Characteristics

What are the main features of Murata's small energy device?

(1)High rate charge-discharge
Murata's small energy device has Low ESR of 800mohm and 10C(30mA) high rate charge-discharge characteristic. It is enabled by optimizing product material and structure.
(2)High safety
No thermal runaway occurs because discharge capacity is small and chemically stable materials are used for Murata's small energy device.
(3)Long cycle life
Charge(Capacity) recovery is over 80% even after 3000 cycles. It enables maintenance free system.

For more details, please visit the product pages.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send