Small Energy Devices FAQ

Characteristics

What are the differences between Murata's small energy device and conventional lithium ion secondary batteries?

Murata's small energy device has following features compared to conventional lithium ion secondary batteries.:

(1)Quick charge/discharge
(2)Long life
(3)Can be operated at low/ high temperatures
(4)High resistance to excessive voltage

For more details, please see the technical note "4.2 Advantages compared to conventional Li-ion secondary batteries".

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send