Small Energy Devices FAQ

Characteristics

What is the recommended charge voltage?

If charge voltage is low, Murata's small energy device cannot be charged to the expected capacity even when it is charged for a long time. Recommended charge voltage is from 2.45V to 2.7V for charging Murata's small energy device to over 80% of its rated capacity.

Charge voltage dependence

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send