Small Energy Devices FAQ

Characteristics

What is the cut-off voltage?

Recommended cut-off voltage at which Murata's small energy device can provide enough performance is 1.8V. However, even if it is stored for a long time at 0V(on a short circuit condition) or excessively discharged to 0V some dozens times, it can be charged again.


For more details, please refer to the technical note "4.2.4 Resistant to excessive discharge".


We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send