Small Energy Devices FAQ

Characteristics

How long can a small energy device be discharged?

Murata's small energy device can be discharged for one hour at 1C(3mA). The higher the discharge current becomes, the shorter the discharge time becomes. Please refer to the following graph for discharge rate dependence.

Discharge current characteritics

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send