Small Energy Devices FAQ

Environment

Are small energy devices compliant with EU RoHS Directive and Halogen-free?

Yes, Murata's small energy devices are compliant with EU RoHS Directive and Halogen-free(*). 

(*) Murata's Halogen-free definition is as below;
1. Chlorine(Cl): <900ppm 
2. Bromine(Br): <900ppm 
3. Total amount of Chlorine and Bromine <1500ppm

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send