Small Energy Devices FAQ

Environment

Is there any regulation on transportation of Murata's small energy device?

Murata's small energy devices are a kind of lithium ion battery. They are proven to meet the requirements of each test in the UN Manual of tests and Criteria, Part Ⅲ, sub-section 38.3. Therefore, in the case of air transportation, the packing standard of the Section II of PI965 (Packing Instruction 965) IATA dangerous materials rule (IATA-DGR) is applied. Please consult with us when air transportation is needed. In addition, please follow regulations of each country.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send