Small Energy Devices FAQ

Mounting

Is there any precautions when applying resin coating to a small energy device?

If coating/molding Murata's small energy device with resin, there is a risk that some resins may erode metal, or cure-stress of resin may distort terminal or package shape. Therefore please pay careful attention in selecting resin. Prior to use, please make the reliability evaluation with small energy devices mounted in your set.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send