Small Energy Devices FAQ

Quality/Reliability

What is the deterioration mode and failure mode of Murata's small energy device?

There are two deterioration modes. One is ESR(internal resistance) increase and the other is capacity decrease.
The failure mode is an open circuit condition.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send