Small Energy Devices FAQ

Quality/Reliability

How long is the lifetime(cycle number)?

In the case of 33C(100mA) charging and 1C(3mA) discharging cycle at 25℃, the capacity recovery rate after 3000 cycles is over 80%.

Charge-discharge cycle characteristics

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send