小型エネルギーデバイスのFAQ


品質/信頼性

What conditions should I store Murata's small energy device?

Please keep product under the following conditions in sealed package.
Temperature: 5-35ºC
Humidity: No more than 70%RH. No condensation.
Avoid any acidic or alkaline environment.
Avoid excessive external force on this product while in storage. 

Even when this device is stored for a long time at 0V(on a short circuit condition) , it can be charged again.
For more details, please refer to the technical note "4.2.4 Resistant to excessive discharge".

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send