Sounders FAQ

Precautions on Using

Are there any points to be aware of handling Piezoelectric Sounders and Piezoelectric Buzzers?

If you put something like a bar in the emitting hole of the product, there is a possibility to cause cracks in the piezoelectric ceramic. Please don't put something like a bar in the emitting hole, because it cause no sound or small sound.
cause cracks

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send