PTC Thermistors (POSISTOR®) FAQ

Mounting

[PTFL/PTFM Series] Are there any precautions to take when packaging "POSISTOR®" with resin?

Heat expands and contracts resin, applying stress to the "POSISTOR®" element. Therefore, elastic resin (resin with high heat conductivity such as those with silicone) must be used. Thoroughly evaluate whether the resin can be used, and then contact us.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send