Ceramic Resonators (CERALOCK®) FAQ

Characteristics

Please explain “the oscillation start up time” of CERALOCK®.

“Oscillation start up time” means the period that the oscillation start moves from a transient state when the IC is activated. Murata defines as the time to reach 90% of the oscillation level under steady state conditions.

“Oscillation start up time” is primarily a function of the oscillation circuit design.
Generally “Oscillation start up time” of CERALOCK® is more than 10 times faster than conventional crystal.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send