Ceramic Resonators (CERALOCK®) FAQ

Characteristics / Mounting

Is there any problem if CERALOCK® is mounted in opposite direction?

In case of mounting CERALOCK® in opposite direction, maximum 0.1% of frequency correlation may occur.
Customized part of tight tolerance series is made by adjustment of frequency on customer’s PCB. However, if you put it in opposite direction, it may be not able to meet required frequency tolerance. 
Please pay attention to the mounting direction when you mount CERALOCK® on your PCB.

Related FAQs
Most people who viewed this page also referred to the following pages.
Q.
Does CERALOCK® have orientation?
Q.
Why does frequency correlation occur when CERALOCK® is mounted in opposite direction?
Q.
What are the meanings of the Marking?

To Ceramic Resonators (CERALOCK®) product page >

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send