Ceramic Resonators (CERALOCK®) FAQ

Precautions on Using

What are the risks when external stress is applied to a lead type CERALOCK®?

This product consists of a hollow structure with an internal space for vibration, and holds the elements on both ends.
If excessive force is applied to the product body while handling or mounting the product, chipping or cracking may occur in the internal elements. Be careful not to apply excessive force to the product body while handling or mounting.

Product cross section (View from top)


Note:Structural Drawings of  Timing Devices
Structure drawings are provided on our website "my Murata®". 
"my Murata®" requires registration for access, and can be found through the following link. https://my.murata.com/en/home (Entry is Free)

We hope that the utilization of "my Murata®" is advantageous so we may innovate together !

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send