June 26, 2009
Murata Manufacturing Co., Ltd.
President/ Statutory Representative Director: Tsuneo Murata

Murata Manufacturing Co., Ltd. has both increased capacitance and reduced cost for X2 capacitors*2 (GB series) certified by the safety standard*1 for power supply primary circuits. This is the first product to achieve 56nF*3 capacitance as a monolithic capacitor aimed at power supply primary circuit application. The cost was also reduced by 15% over the previous model by replacing precious metal used for electrodes with base metal. This product can reduce the unit volume to 1/10 when replacing the typical choice of film capacitors for power supply primary circuits. The unit volume reduction makes the product ideal for small and low profile equipment such as adaptors for note-size PCs.
Safety standard is required for capacitors used in power supply primary circuits due to the risk of being exposed to high-voltage surge. Film capacitors typically used for this application were generally large and were not heat-resistant. The recent trend for smaller electronic equipment created demands for smaller capacitors for power supply primary circuits. Murata met these demands by developing the GB series certified by the safety standard for monolithic ceramic-type capacitors which can be made smaller than film capacitors and have been mass produced since 2003. Replacing precious metals like silver used for electrodes with base metals like nickel reduced previously high production costs. Simultaneously, the range of capacitance was increased from 10 - 33nF to 10 - 56nF to meet the need for high capacitance in X2 capacitor applications.
*1 Safety standard
Standard or regulation to ensure prevention of hazards caused by electronic equipment and components
*2 X2 capacitors
Capacitors satisfying class X2 safety standard against voltage surge etc., connected to power supply primary circuit lines (between hot and neutral conductive paths). For removing normal mode noise causing electro-magnetic interference.
*3 nF
1 billionth of a farad
Capacitor to prevent electromagnetic interference used for power supply primary circuit X2 capacitor application
| Model | Series | Nominal capacitance (nF) | Part No. |
|---|---|---|---|
| GA355 (5.7×5.0) | GB | 10 | GA355QR7GB103KW01L |
| 15 | GA355QR7GB153KW01L | ||
| 22 | GA355DR7GB223KW01L | ||
| 33 | GA355ER7GB333KW01L | ||
| 47 (new) | GA355ER7GB473KW01L | ||
| 56 (new) | GA355XR7GB563KW06L |

| g | 3.0mm |
|---|---|
| L×W | 5.7×5.0mm |
| T | 1.5mm~2.9mm (Changed by the product number) 1.5mm … 10 and 15nF capacitance models 2.0mm … 22nF capacitance model 2.5mm … 33nF and 47nF capacitance models 2.9mm … 56nF capacitance model |
500 thousand units per month starting April 2009
50Yen/per unit (Varies by the product number)
This is a PDF file. Adobe Reader is required to view, print, or download this file.
This document file is in RSS (XML) format. An "RSS reader" is required to read this file.