Global / MURATA MANUFACTURING CO., LTD.
Help

Murata Commences Mass Production of World’s Smallest Bluetooth® Modules in its "LBMA Series"; Cumulative "LBMA Series" Production Passes 500 Million Mark

March 31, 2010

Murata Manufacturing Co., Ltd.
President/ Statutory Representative Director: Tsuneo Murata

Murata Commences Mass Production of World’s Smallest Bluetooth® Modules in its "LBMA Series"; Cumulative "LBMA Series" Production Passes 500 Million Mark

Overview

Murata Manufacturing Co., Ltd. has begun mass production and shipment of the world’s smallest Bluetooth® modules in its “LBMA Series”. With dimensions of 3.5x3.5mm, these modules are 30% smaller than past products.

Additionally, in the ten years since initiating the mass production of the LBMA series in March of 2000, Murata has produced in excess of 500 million units, the highest cumulative production volume of Bluetooth® modules in the world.

Background

With the ever increasing functionality of mobile phones, there is a demand for smaller, increasingly high performance, and increasingly high quality mobile phone components, devices, and modules. Additionally, the dramatic spread of the Internet has spurred a demand for mobile Internet devices with functions similar to those of mobile phones.

In March of 2000, Murata initiated the first successful mass production of Bluetooth® modules aimed at the European mobile phone market, but this time, in an effort to respond to the market’s demand for smaller products, we have made use of our company’s original ceramic substrate, high frequency design/evaluation technologies, and miniaturization technologies to begin the mass production of the world’s smallest Bluetooth® modules. With dimensions of 3.5x3.5mm, these modules represent an approximately 30% reduction in size over our most recent Bluetooth® module product.

Furthermore, in the ten-year period from the initiation of LBMA Series mass production in March 2000 to the present time of March 2010, Murata has produced 500 million units, the world’s highest cumulative production volume of Bluetooth® modules, with this new 3.5x3.5mm product representing an over 90% reduction in size over the original 14x10mm model.

With an approximately 90% share of the worldwide mobile phone Bluetooth® module market, Murata leads the world in the production of Bluetooth® modules. Through our continued development of small, high performance wireless modules, we will work to contribute to the increased functionality of devices.

Features

  • World’s smallest size (3.5x3.5x1.0mm) (an approximately 30% reduction in size over past products)
  • Achieves high performance and high quality (high reliability) through advanced high frequency design technology
  • Achieves excellent electromagnetic wave resistant characteristic through Murata’s original packaging technology
  • Does not use substances controlled by the RoHS directive

Applications

  • mobile phone
  • portable music player
  • PMP (Portable Media Player)
  • PND (Portable Navigation Device)
  • digital photo frame
  • MID (Mobile Internet Device)

Part Number

  • LBMA Series (Bluetooth® Module)
  • LBED Series (Bluetooth®+FM Combo Module)
  • LBEE Series (Bluetooth®+Wi-Fi® Combo Module)
  • LBEH Series (Bluetooth®+Wi-Fi®+FM Combo Module)
  • LBEF Series (Bluetooth®+GPS+FM Combo Module)
  • LBEH Series (Bluetooth®+GPS+FM Combo Module)

Electric Characteristics

LBMA43PQN

Bluetooth Specification Ver2.1+EDR
Supply Voltage 3.3V
Output Power 0dBm (Class2)
Sensitivity -79dBm
HOST Interface UART

Production

20 million units per month in March 2010

  • Bluetooth is a registered trademark of Bluetooth SIG, Inc.
  • “Wi-Fi” is a registered trademark of the Wi-Fi Alliance
NOTE

This is a PDF file. is required to view, print, or download this file.

This document file is in RSS (XML) format. An "RSS reader" is required to read this file.

Contact Us

Advertisement

About RSS Feed

CSR Activities

Home > News > News Release > 2010 > Murata Commences Mass Production of World’s Smallest Bluetooth® Modules in its "LBMA Series"; Cumulative "LBMA Series" Production Passes 500 Million Mark

Help

Global / MURATA MANUFACTURING CO.,LTD.