Jul 16, 2010
Murata Manufacturing Co., Ltd.
President/ Statutory Representative Director: Tsuneo Murata
Murata Manufacturing Co., Ltd. has developed a platform of highly efficient power supplies for the industrial equipment market. These products exhibited at the TECHNO-FRONTIER 2010 show to be held at Tokyo Big Sight from July 21-23.
As interest in environmental conservation continues to grow, measures to conserve energy and resources are being demanded not only for electronic equipment used in households and offices, but also for industrial equipment.
Murata Manufacturing has a proven track record for developing highly efficient, long-life customized power supplies for printers, facsimile machines, and a variety of digital AV equipment. Based on its success and expertise in power supply circuit technology in these areas, Murata Manufacturing has decided to create a new platform of AC-DC power supplies for industrial equipment
This new platform, the MVB series, currently consists of two products of the table, and Murata Manufacturing intends to further develop and expand the lineup to include other models in the future.
| Product name | MVBA150-12□□□ | MVBB300-24□□□ | MVBA150-24□□□* |
|---|---|---|---|
| Input voltage | 85~264VAC | ||
| Output voltage | 12V | 24V | 24V |
| Maximum power capacity | 150W | 300W | 150W |
| Efficiency (at 100V) |
86% | 88% | 88% |
| (at 200V) | 88% | 91% | 90% |
| Size | 93×34×168mm | 120×40×250mm | 93×34×168mm |
* We are planning to commercialize of MVBA150-24□□□* in the second semester of 2010.
91.5% at AC240V 300W

Semiconductor manufacturing equipment, various measuring and analysis devices, industrial robot equipment, LED display devices, and other industrial equipment
Production began April 2010.
2 patents pending
| Period | July 21 (Wednesday) to July 23 (Friday), 2010 |
|---|---|
| Venue | Tokyo Big Sight |
| Murata Manufacturing booth No | 3V-201 25th Power Supply System Exhibit 2N-101 23rd EMC/Noise Countermeasure Technology Exhibit 2L-106 12th Heat Countermeasure Technology Exhibit 3Y-207 Centralized Exhibit - Energy Harvesting Zone |
This is a PDF file. Adobe Reader is required to view, print, or download this file.
This document file is in RSS (XML) format. An "RSS reader" is required to read this file.