May 16, 2011
Murata Manufacturing Co., Ltd.
President/ Statutory Representative Director: Tsuneo Murata

Murata Manufacturing Co.,Ltd. is proud to announce that it has created a series of chip monolithic ceramic capacitors which feature metal pins and which are designed to be used in automotive electronic devices.
These capacitors will be showcased in Murata’s booth at the Automotive Engineering Exposition scheduled to be held at PACIFICO Yokohama starting on May 18.
In the automotive market, the automakers, stimulated by the increasing interest focused in recent years on tackling global environmental problems and energy problems, have been pushing hard to develop hybrid electric vehicles (HEV) and electric vehicles (EV) and promote their practical use.
When chip monolithic ceramic capacitors (MLCC) - and especially large ones - are used in the automotive electronic devices installed on these HEVs and EVs, they are easily affected by the stress of the expansion and contraction of the substrates generated by sharp temperature changes, and under conditions where they will be exposed to thermal shock*1 occurring over long periods of time, measures to deal with solder cracks are an absolute necessity. Similarly, measures to deal with cracks in the capacitor elements that form as a result of vibration and mechanical impact must also be taken, and the capacitors are required to exhibit a higher level of reliability than when they are used in general - purpose products. So providing the capacitors with metal pins that have an elastic action reduces the impact to which the capacitor elements are subjected.
DC - DC converters in automotive ECUs*2, etc.
| *1 Thermal shock: | Sudden or abrupt changes in the ambient temperature |
|---|---|
| *2 ECU: | Electronic control unit - the computer that electronically controls the devices or systems in a motor vehicle |
* "****" denotes a 4 - digit number provided by Murata.
| Rated voltage (DC) |
Length (L) x width (W) (mm) |
Height (T) (mm) | Temperature characteristics | Static capacitance | Static capacitance tolerance | Murata model number |
|---|---|---|---|---|---|---|
| 25V | 6.1x5.3 | 3.7±0.2 | X7R | 22uF | ±10% | KCM55QR 71E226K**** |
| 6.1x5.3 | 6.4±0.3 | X7R | 47uF | ±20% | KCM55WR 71E476M**** |
|
| 35V | 6.1x5.3 | 3.7±0.2 | X7R | 17uF | ±10% | KCM55QR 7YA176K**** |
| 6.1x5.3 | 6.4±0.3 | X7R | 33uF | ±20% | KCM55WR 7YA336M**** |
|
| 50V | 6.1x5.3 | 3.7±0.2 | X7R | 10uF | ±10% | KCM55QR 71H106K**** |
| 6.1x5.3 | 6.4±0.3 | X7R | 22uF | ±20% | KCM55WR 71H226M**** |
|
| 63V | 6.1x5.3 | 3.7±0.2 | X7R | 10uF | ±10% | KCM55QR 71J106K**** |
| 6.1x5.3 | 6.4±0.3 | X7R | 22uF | ±20% | KCM55WR 71J226M**** |
|
| 100V | 6.1x5.3 | 2.8±0.2 | X7R | 4.7uF | ±10% | KCM55LR 72A475K**** |
| 6.1x5.3 | 4.8±0.2 | X7R | 10uF | ±20% | KCM55TR 72A106M**** |
| Test temperature: | -55 to +125 degrees Celsius |
|---|---|
| Time left standing: | 5 minutes at each temperature level |
| Substrate used: | Glass epoxy substrate (FR - 4) |

| Chip size | Discrete chip (5,750 size) |
Capacitor with metal pins (5,750 size) |
|---|---|---|
| 1,000 cycles | ![]() |
![]() |
| 2,000 cycles | ![]() |
![]() |
Fig. 1 Comparison of solder cracks generated by thermal stress (liquid bath test)
Fig. 2 Substrate warping test comparison
Fig. 3 Outline drawing (1 - level product)
Fig. 4 Outline drawing (2 - level product)
* The height (T) differs from one model number to another. For further details, refer to the [Parts number table].
Mass production scheduled to commence in July 2011
| Dates: | Wednesday, May 18 to Friday, May 20 |
|---|---|
| Venue: | PACIFICO Yokohama |
| Murata booth No. : | 222 |
| URL: | http://www.murata.com/event/autoee2011/index.html |
This is a PDF file. Adobe Reader is required to view, print, or download this file.
This document file is in RSS (XML) format. An "RSS reader" is required to read this file.