July 4, 2011
Murata Manufacturing Co., Ltd.
President/ Statutory Representative Director: Tsuneo Murata
Murata Manufacturing Co., Ltd. recently earned UQ certification*1 for its WiMAX*2 communication module (LBFA1ZRSTZ) after its module had successfully completed the network connectivity testing of UQ Communications Inc. ("UQ" below) .
"UQ certification" is required when communication products are to be connected to the UQ networks that use the "WiMAX" wireless standard, and if a module that has acquired UQ certification is installed, the number of items to be tested in the end - product can be significantly reduced, and the time and trouble involved in testing and certifying the end - product can be lessened. In addition, this certification greatly shortens the development period of the products.
The door is now open for Murata Manufacturing to supply not only WiMAX module hardware, but even the drivers and communication middleware. The equipment manufacturers, who are the company's customers, can now achieve WiMAX functions for their products simply by preparing the user interfaces and applications. Murata also offers services to acquire various kinds of certification needed for the end - products.
In the future, WiMAX communication functions are expected to be featured in smart phones and PCs as well as in all kinds of portable communication devices. Murata's miniaturization technology — and its WiMAX Module (LBFA1ZRSTZ) is a typical example of what this technology can accomplish — will be making an important contribution to opening up the WiMAX - related market.
Smart phones, cell phones, mobile PCs, etc.
The new WiMAX communication module from Murata Manufacturing has been developed by virtue of the company's high - grade miniaturization technology, and it is the smallest WiMAX module available. Together with Murata, we at UQ Communications wish to promote the increasing adoption of WiMAX communication functions in compact communication products. We are also striving to offer a greater array of services and expand this whole business area, and we will continue to propose new possibilities for WiMAX.
| *1 UQ certification | This program, provided by UQ Communications Inc., certifies that the WiMAX communication product concerned has successfully completed testing for connectivity with the WiMAX networks of UQ Communications. Due to the fact that Murata's WiMAX communication module (LBFA1ZRSTZ) has now acquired this certification, the number of man - hours involved in testing connectivity with the WiMAX networks of UQ Communications in the end - products that incorporate this module can be drastically reduced. |
|---|---|
| *2 WiMAX | This is a wireless communication standard. It offers high - speed and large - capacity wireless broadband communications. |
LBFA1ZRSTZ
16.8mm x 20.4mm x 2.3mm
Komatsu Murata Manufacturing Co., Ltd.
10,000 yen per unit
This is a PDF file. Adobe Reader is required to view, print, or download this file.
This document file is in RSS (XML) format. An "RSS reader" is required to read this file.