February 15, 2012
Murata Manufacturing Co., Ltd.
President/ Statutory Representative Director: Tsuneo Murata
Murata Manufacturing Co., Ltd. has successfully developed the world's smallest micro DC-DC converter.*
The line-up has been expanded to include four series; expanded sales have been started.
Furthermore, some series are already installed in SmartPhones.
*Refers to LXDC2UR series: 2.5 mm x 2.3 mm (supports up to 0.6 A) ; LXDC3EP series: 3.5 mm x 3.2 mm (supports up to 1.0 A) .
The micro DC-DC converter features ultra-compact size and suppression of EMI noise. We are certain that this converter will greatly contribute to miniaturizing mobile devices while they continue to provide even greater functionality.

As electronic devices have increasingly powerful functionality, it has become necessary to supply power individually over each feature circuit. To support needs in the marketplace, we have successfully developed and commercialized for the first time, in October 2010, a micro DC-DC converter. Our success is the result of applying our unique circuit design engineering and multi-layer processing engineering. Marketplace needs include:
Currently, we are providing a line-up that includes a total of four series to start expanding sales. These series include the world's smallest devices that support even further miniaturization, high-current components that handle up to 3.0A, and voltage step-up types. We will continue to work on developing products that are ultra-compact, and have low EMI noise, to contribute to optimization of power-surrounding circuit designs.
All mobile devices such as SmartPhones and the like.
| Series Name | Type | Size | Capacity | External View |
|---|---|---|---|---|
| LXDC2UR Series |
Voltage step-down type |
World's Smallest! 2.5 x 2.3mm |
0.6A | ![]() |
| LXDC3EP Series |
Voltage step-down type |
World's Smallest! 3.5 x 3.2mm |
1.0A | ![]() |
| LXDC55B Series |
Voltage step-down type |
5.7 x 5.0mm | Supports High Currents! 3.0A |
![]() |
| LXDC44A Series |
Voltage step-up type |
4.0 x 4.0mm | 0.7A | ![]() |
See the Selection Guide of Micro DC-DC Converters.
Starting mass production sequentially at Okayama Murata Manufacturing Co., Ltd. from October 2011.
3 patents granted
5 patents pending
This is a PDF file. Adobe Reader is required to view, print, or download this file.
This document file is in RSS (XML) format. An "RSS reader" is required to read this file.