Global / MURATA MANUFACTURING CO., LTD.
Help

Capacitors

FAQ of Polymer Capacitors

What is a Murata polymer aluminum electrolytic capacitor?

There are two kinds of polymer aluminum capacitors: the “surface mount” type (also known as H-Chip), which uses a multilayer aluminum foil structure, and the “Can” type (also known as V-Chip), which consists of a rolled aluminum structure.
Murata's H-Chip type (ECAS Series) is designed with a resin molded case structure, which utilizes multilayer aluminum foil for anode and solid conductive polymer for negative cathode.

Al Capacitor

There are two kinds of polymer aluminum capacitors: the “surface mount” type (also known as H-Chip), which uses a multilayer aluminum foil structure, and the “Can” type (also known as V-Chip), which consists of a rolled aluminum structure.

Top of Page

Is the ECAS series a multi-layer device?

Yes. The ECAS series utilizes multilayer aluminum foil for anode and solid conductive polymer for negative cathode.

Yes. The ECAS series utilizes multilayer aluminum foil for anode and solid conductive polymer for negative cathode.

Top of Page

What are the advantages of using polymer aluminum capacitors vs other non-ceramic technologies?

ESR and impedance of Murata’s polymer capacitor are lower than other non-ceramic type capacitors because a multilayer structure design uses a conductive polymer for cathode; therefore, the ECAS series exhibits high performance for noise suppression, ripple absorption, and decoupling.

ESR and impedance of Murata’s polymer capacitor are lower than other non-ceramic type capacitors because a multilayer structure design uses a conductive polymer for cathode; therefore, the ECAS series exhibits high performance for noise suppression, ripple absorption, and decoupling.

Top of Page

What are the advantages of using polymer capacitors vs MLCC?

MLCCs offer the best overall solution in terms of size, volumetric capacitance, and low impedance.
Polymer capacitors extend the high capacitance offering.

MLCCs offer the best overall solution in terms of size, volumetric capacitance, and low impedance.

Top of Page

Do polymer electrolytic capacitors have polarity?

Yes. Unlike MLCCs, polymer electrolytic capacitors have a marked polarity so proper placement on the PCB board is important.

Yes. Unlike MLCCs, polymer electrolytic capacitors have a marked polarity so proper placement on the PCB board is important.

Top of Page

Can the ECAS series be used in AC circuits?

No, because these components have polarity.

Top of Page

Is voltage derating required for ECAS capacitors?

No. Murata's ECAS capacitors can be used without voltage derating because the electrolytic formation voltage is higher during manufacturing.

Top of Page

What is the operating temperature range of Murata's ECAS series?

Operating temperature range is: -40℃ to 105℃

Top of Page

What is the capacitance and voltage range of the ECAS series?

Capacitance range is 6.8µF to 470µF Rated voltage range is 2VDC to 16VDC

Top of Page

Can the ECAS series be exposed to reflow and wave soldering environments?

The ECAS series can only be reflowed soldered. Please check our specifications for applicable profiles and conditions.

Top of Page

Are there special handling and storage conditions required for the ECAS series?

No. The ECAS series are rated at MSL 3 and are packaged in special packaging and can be stored under normal warehouse conditions.

Top of Page

Do polymer electrolytic capacitors experience the same capacitance changes under applied voltage like MLCCs?

No. Polymer electrolytic capacitors do not exhibit “dc bias” characteristics shown by class 2 or 3 (high K) MLCC.

Top of Page

What is the average reel size of the ECAS series?

  • Case Size D4 (T=1.9mm/size is 3000pcs/reel @ ø 330mm)
  • Case Size D6 (T=2.8mm/size is 2500pcs/reel @ ø 330mm)
  • Case Size D9 (T=4.2mm/size is 2000pcs/reel @ ø 330mm)

Top of Page

Will the ECAS product continue to follow Murata's 18 digit global part numbering (GPN) system?

Yes. The ECAS series will follow Murata's conventional 18 digit GPN system.

品番体系

Top of Page

Why did Murata enter the polymer capacitor business after being in MLCCs for so long?

Our strategy and goal have been to become a complete capacitor solution provider.

Top of Page

Back to "FAQ"
Home > Products > Capacitors > FAQ > Polymer Capacitors

Help

Global / MURATA MANUFACTURING CO.,LTD.