Global / MURATA MANUFACTURING CO., LTD.
Help

Home > Products > Capacitors > Proposal of New Tape Packaging > Bulk Feeding System > Circuit Designs Best Suited to Bulk Feeding

Capacitors

  • Inquiries
  • PDF Catalogs
  • NetWork - Global

Bulk Feeding System

Circuit Designs Best Suited to Bulk Feeding

To maximize the benefits generated by using the bulk feeding system, it is important to consider the process from the circuit design stage.

Unify the component size to "0402C" or "0603C".

  • Unifying the component size enables only a single kind of bulk feeder to be used. This makes it easier to control the bulk feeding system.
  • For "0805C" or larger sized components, the component thickness will vary, requiring two or more bulk feeders. Because "0402C"- or "0603C"-size components have the same size and shape, one type of bulk feeder can be applied to a wide variety of products. For such small sized chip monolithic ceramic capacitors, our company offers various products ranging from those with minute capacitance to those with large capacitance. Contact us for details.

Contact Us (Products and Personnel) Form

Unify the capacitance value to "E1 step".

  • As far as possible, use components that have the same capacitance value and temperature characteristic. If these values are standardized, great effects can be achieved when using the bulk feeding system.
    By using many "E1 step (*)" group products, whose unit price is relatively low, the cost of equipment production can be dramatically reduced.

*)"E1 step" products: Products with a capacitance value of 10pF, 100pF, 1,000pF, or 0.01µF...

Do not specify the packaging style in the circuit design stage.

  • If the packaging style is specified in the circuit design stage, taping-packaged components cannot be changed to bulk-packaged ones in the mounting process. Likewise, bulk-packaged components cannot be changed to taping-packaged ones either. If specifying only taping packaging as the packaging style, the bulk feeding system cannot be used in the mounting process. And if specifying only bulk packaging as the packaging style, taping-packaged components cannot be used if problems occur during bulk feeding. By not specifying the packaging style in the circuit design stage, greater flexibility is possible because the packaging style can be selected during the mounting process based on the situation.
Home > Products > Capacitors > Proposal of New Tape Packaging > Bulk Feeding System > Circuit Designs Best Suited to Bulk Feeding

Help

Global / MURATA MANUFACTURING CO.,LTD.