Global / MURATA MANUFACTURING CO., LTD.
Help

Home > Products > Capacitors > Proposal of New Tape Packaging > Bulk Feeding System > Global Environmental Protection

Capacitors

  • Inquiries
  • PDF Catalogs
  • NetWork - Global

Bulk Feeding System

Global Environmental Protection

Reducing the amount of paper resources used

The bulk feeding system contributes toward protecting the environment by greatly reducing the amount of paper resources used.

Components of taping packaging (percentage by weight)

When checking the construction of taping packaging, it is found that 80% of the packaging material is composed of paper tape. The function of the paper tape is to keep electronic components lined up. However, after components have been used, the paper tape is typically discarded. Since plastic tape is also being used for taping packaging, it is common for paper and plastic tapes to sometimes be mixed together, making recycling difficult.

Components of taping packaging (percentage by weight)

Amount of paper resources used according to type of packaging

The bulk feeding system helps protect the environment by reducing the amount of paper resources used, to only 1/40 to 1/20 that of previous products (compared with our products).

The bulk case is designed as a packaging material that can be reused or recycled. If the bulk case can maintain the performance of the electronic component packaging materials, it can be reused. But if the performance of the case's packaging material is lost, the bulk case is broken down and recycled.

Amount of paper resources used according to type of packaging

Saving the energy used for transportation

1/40 of that used for taping packaging The numeric values shown above are calculated based on "0402"-size components.

Saving the energy used for transportation
Home > Products > Capacitors > Proposal of New Tape Packaging > Bulk Feeding System > Global Environmental Protection

Help

Global / MURATA MANUFACTURING CO.,LTD.