Basic Knowledge

Explanation of function and how to use inductors.
(EMICON-FUN!)

Inductor's Function

Explanatoin of summery of inductor.

What is RF Inductor?

The features of RF inductors and how they can be applied.

What is Inductor for Power Lines?

The features of RF inductors and how they can be applied.

Basic Structure and Features

Explanation of difference in application and feature according to structure.

How to Test Inductor

Explanation of matters that require attention with past examples when mounting inductors.

Why are there two kinds of rated current for power lines?

There are two kinds of rated currents of power inductor. Do you have any question about those differences?
Here we explain on the rated current of the power inductor.

Why do inductors have a directional mark?

Explanation of inductor and the influence of the magnetic field.