Explanation of function and how to use inductors.
Explanatoin of summery of inductor.
The features of RF inductors and how they can be applied.
The features of RF inductors and how they can be applied.
Explanation of difference in application and feature according to structure.
Explanation of matters that require attention with past examples when mounting inductors.
There are two kinds of rated currents of power inductor. Do you have any question about those differences?
Here we explain on the rated current of the power inductor.
Explanation of inductor and the influence of the magnetic field.