Global / MURATA MANUFACTURING CO., LTD.
Help

Resonators

Basic Knowledge of Ceramic Resonators "CERALOCK®"

Oscillation

Generally, oscillations circuits fall into the following three classes:

  • Positive feedback
  • Negative resistance
  • Transmission time or phase delay

Of the above circuits, the "CERALOCK®", quartz resonators and LC circuits use the first method. Colpitts circuit and Hartley circuit are typical examples of LC positive feedback and tuned antibonding oscillation circuit, see below.

<Colpitts circuit>

Colpitts circuit

<Hartley circuit>

Hartley circuit

The above circuits use the most fundamental transistors as amplifiers. The oscillation frequency of the Colpitts and Hartley circuit is approximately the same as the resonant frequency of the circuit comprised of L, CL1 and CL2 and that of the circuit comprised of L1 and L2, respectively. The oscillation frequency of these circuits is individually expressed by the following formulae:

<Colpitts circuit>

Colpitts circuit

<Hartley circuit>

Hartley circuit

To use the "CERALOCK®" in the LC circuit, replace "L" of the LC circuit with the "CERALOCK®" by utilizing the inductance between "fr" and "fa." Generally, the "CERALOCK®" is replaced with "L" of the Colpitts circuit.
The operating principle of the oscillation circuit is described below. In the feedback circuit as shown on the right, its oscillating conditions are as follows:

Loop gain

The Colpitts circuit uses an inverting amplifier (theta1=180°), and also uses "L" and "C" in the feedback circuit for further inversion (theta2=180°). When the "CERALOCK®" is used in the oscillation circuit, it is based on the same operating principle. To build the Colpitts oscillation circuit using the "CERALOCK®", the method of using an inverter is most commonly and easily available.

Loop gain

Top of Page

Back to "Resonators"

Basic Knowledge of Ceramic Resonators "CERALOCK®"

Home > Products > Resonators > Basic Knowledge > Ceramic Resonators "CERALOCK®" > Oscillation

Help

Global / MURATA MANUFACTURING CO.,LTD.