Basic Knowledge of Magnetic Pattern Recognition Sensors
Testing Methods
For detailed information on individual products, jump from "Characteristics" to the Search Engine.
Sensor Noise Testing Method
This testing method is used to measure the noise generated from the sensor.
Testing Circuit
Testing Methods
- Measure noise by using the measuring circuit with an oscilloscope. The head surface must be free from magnetism. (Do not place a magnetic object near the head surface.)
- The measuring range of the oscilloscope is 0.5V/DIV or 50ms/DIV.
- To prevent static electricity from the body from affecting the measurement results, the person who conducts this test should wear an earth band.
Top of Page
Piezoelectric Noise Testing Method
Piezoelectric noise is a voltage generated between both ends of an element (resistor) when external stress is applied to the element (resistor). The element is protected by a space between the element and case, so that external forces will not affect the measurement results.
Testing Circuit
The sensor noise measuring circuit is used.
Testing Methods
- A card is scanned with the sensor's detecting surface, as shown below:
- Apply 5±0.1VDC to the sensor, and apply 98mN spring load to the transport roller. Through the sensor noise measuring circuit (gain: x 10,000), measure the voltage generated when the card is transported at a speed of 2mm/s.
Top of Page
Back to "Basic Knowledge"
Basic Knowledge of Magnetic Pattern Recognition Sensors