Global / MURATA MANUFACTURING CO., LTD.
Help

Sensors

Principles of Magnetoresistive Elements

Magnetoresistive Elements

Semiconductor Materials for Magnetic Sensors

Murata magnetic sensors use magnetoresistive elements made of n-InSb (compound semiconductor of the III-V group).

Material property InSb InAs GaAs Ge Si
Crystalline structure Concentrated zinc ore Concentrated zinc ore Concentrated zinc ore Diamond Diamond
Band gap (eV) 0.17 0.36 1.43 0.66 1.12
Electron mobility (cm2/V s) 78000 33000 8500 3900 1900
Hole mobility (cm2/V s) 750 450 450 1900 425
Melting point (°C) 525 943 1237 953 1420
Density (Kg/m3) 5.775 5.67 5.316 5.35 2.3
Lattice constant (Å) 6.48 6.06 5.64 5.66 5.43
Resistivity (ohm cm) 5 x 10-3 3.1 x 10-1 3.8 x 108 - -
  • n-InSb materials with high electron mobility are used for the magnetoresistive elements.
  • InAs, GaAs, Ge, Si, and InSb materials are used for the Hall elements and Hall ICs.

Top of Page

Structure of the Magnetoresistive Element

The magnetoresistive element has two terminals. The element for practical use is formed like meanders by means of photolithography, so that it has multiple electrodes on the semiconductor surface to provide high resistance and high output.

Element Model (meander-formed element)

Element Model
  • By modifying the shape of the element, a wide range of resistances can be achieved.
  • An element is formed on a magnetic or non-magnetic substrate, depending on its usage. If the priority is high output, a magnetic substrate is used. If the priority is immunity to external magnetic noise, a non-magnetic substrate is used.

Top of Page

Magnetic Flux Density/Resistance Change Characteristic

As expressed by the formula Rb = R0 (B/ (0 [1 + m(micro B)2], the resistance increases non-linearly in the range of low magnetic flux densities, while it increases linearly in the range of high magnetic flux densities.

Magnetic Flux Density/Resistance Change Characteristic

Magnetic Flux Density/Resistance Change Characteristic

  • The resistance increases in proportion to the magnetic flux density, independent of the polarity.
  • The resistance increases non-linearly in the range of 80mT or less magnetic flux densities. When the magnetic flux density exceeds 80mT, the resistance increases linearly.
  • If the magnetic flux density reaches 300mT, it indicates that the resistance has increased approx. four times from the initial resistance.
  • The resistance will not be saturated even at a high magnetic flux density.

Top of Page

Resistance/Temperature Characteristic

The resistance/temperature characteristic depends on the carrier density.

Resistance/Temperature Characteristic

Resistance/Temperature Characteristic

  • 100% corresponds to the resistance obtained at 25°C.
  • The temperature coefficient is high (approx. -2%/°C).

Top of Page

Back to "Sensors"

Principles of Magnetoresistive Elements

Home > Products > Sensors > Technical Guide > Principles of Magnetoresistive Elements > Magnetoresistive Elements

Help

Global / MURATA MANUFACTURING CO.,LTD.