Global / MURATA MANUFACTURING CO., LTD.
Help

Sound Components

FAQ concerning Piezoelectric Speakers

FAQ

Please let me know the features of Piezo Speakers.

Piezo speaker can be an ultra thin device as it generates sound by the flexure vibration of a thin piezo ceramic plate.
Murata offers piezo speakers of variety of thickness ranging from 0.5mm to 1.2mm to suit any of your demand.
Please contact us for more details.
Our catalog is on our website. (PDF:724KB)

Top of Page

What is the difference between Piezo Speakers and Dynamic Speakers?

Dynamic speakers generate sound with vibration of a diaphragm film by utilizing the electromagnetic force of a magnet and a coil, while piezo speakers do only with a thin piezo ceramic plate attached to a diaphragm film by utilizing the piezoelectric vibration of the ceramic itself.
This structure enables piezo speakers to be ultra thin.
Due to the magnet-less structure, piezo speakers are free from iron sand inhalation problem, and have no influence to the magnetic sensors or memory card slots, as they do not generate magnetic field.
In addition, Piezo speakers help expanding the battery life as they generally consume less electrical power than dynamic speakers.

Top of Page

How can I drive Piezo Speakers?

Just like dynamic speakers, you need an audio amplifier to drive piezo speakers, however, those amplifiers designed for dynamic speakers may not be able to generate enough voltage to drive piezo hard enough, resulting the sound not as loud as expected.
As the piezo speakers are voltage-driven type of devices, it is recommendable to take audio amplifiers designed to drive piezo. There are many types of such amplifiers available in the market. Contact us for more assistance if needed.

Piezo Speakers

Top of Page

How is the power consumption of Piezo Speakers?

The electrical power consumption of piezo speakers including drive circuit varies according to the audio amplifier used, however, piezo speakers generally consume less power compared to dynamic speakers.
The combination of piezo speaker and class-D amplifier shows extremely small power consumption.

Top of Page

Do you make waterproof Piezo Speakers?

Yes, we've developed the world’s first waterproof Piezo speaker.
Visit below URL for the news release.

back to FAQ

Top of Page

Sound Components

Home > Products > Sound Components > FAQ > Piezoelectric Speakers

Help

Global / MURATA MANUFACTURING CO.,LTD.