Item to be checked |
Selection criteria |
|
| How much (in volts) is the power supply voltage of the circuit in which "POSISTOR®" is used? (Preventing "POSISTOR®" from being damaged) |
-> | Power supply voltage ≦ Maximum voltage of "POSISTOR®" |
| arrow | ||
| When the circuit is operating normally, how much (in amperes) is the current that flow through "POSISTOR®"? (Preventing "POSISTOR®" from malfunctioning) |
-> | Normal current ≦ Non-operating current of "POSISTOR®" |
| arrow | ||
| When something abnormal such as a short circuit has occurred, how much (in amperes) is the current that flows through "POSISTOR®". (Ensuring reliable protection) |
-> | Abnormal current ≧ Operating current of "POSISTOR®" |