PTC Thermistors are used for the temperature sensor and the current limitation device with the element that increases electric resistance by the rise of the temperature.
Using an excellent material in the heat response, Murata's PTC Thermistors "POSISTOR®" are used to detect overheating, protect circuits in the event of drawing too much current in electronic equipement. Murata offers a variety of thermistor products for the demands of many applications.
NTC Thermistor are used for the temperature sensor with the element that decreases electric resistance by the rise of the temperature.
Using an excellent material in the heat response, Murata's NTC Thermistor are used for inrush current protection, temperature compensation in electronic equipement. Murata offers a variety of thermistor products for the demands of many applications.
Thermistors