murata EnglishChineseJapanese
Region
GlobalNorth AmericaEurope


Home > Trimmer Capacitors > F.A.Q. > TZY2 Series
Advantage of the Design
An improved cover shape prevents flux from penetrating inside.
Advantage of the Design
Advantage of the Design
bullWhen the distance between the stator and cover is very small, capillary phenomenon occurs easily, allowing flux to possibly penetrate inside.

fingerThe cover includes a protrusion which provides a certain distance between the stator and cover. This prevents the flux from penetrating inside due to the capillary phenomenon.
bullWhen solder-containing flux is used, the flux separates from the solder when it melts.

fingerThe cover is designed so that as the flux separates from the solder it is retained in the flux receptacle and prevented from penetrating inside.
UP