AMR Sensors (Magnetic Sensors)Glossary: AMR sensors (magnetic sensors)

A-B-C

Active magnetic field

  • This is the strength of the magnetic force where the AMR sensor turns on (or off), and it is specified in units of mT (millitesla).
  • The ON sensitivity (Hon) is the magnetic force that turns on the sensor which was off with a weak magnetic field, the OFF sensitivity (Hoff) is the magnetic force that turns off the sensor which was on with a strong magnetic field, and H stands for the magnetic flux density.

AMR

AMR is an abbreviation for Anisotropic Magneto Resistance. The AMR sensor has a magnetic force line direction where the magnetic field can be detected and a direction where the magnetic field cannot be detected.

Analog output

  • In most AMR sensors, the output is Hi/Lo digital output and is used for switch applications, but some sensors include products consisting of elements only, and the output voltage is output as an analog signal. These sensors are not for all-purpose applications.
  • Consider a digital output type with an internal processing circuit.

Chattering

Chattering is a state of repetitive switching between on and off under certain conditions. If the supply voltage is adjusted by an external resistor or if no capacitors are available in the area, the voltage may drop at the moment that a large amount of current is used in the internal sampling mode, and the circuit may be unable to turn on. Be aware that, if this situation occurs in a magnetic field around the ON level, repetitive switching will occur between Hi and Lo in the same way as chattering.

Current consumption

  • This is the current used by the AMR sensor to operate.
  • This is the current used when it flows to the IC circuit and magnetic resistors in the sensor.
  • The current consumption depends on the supply voltage. A larger supply voltage results in a higher current consumption.

D-E-F

Elements

  • Elements refer to the analog outputs.
  • In the sensor, analog output is used to detect how the magnet approaches the sensor and the rotating position of the magnet.
    The analog output can provide higher resolution results depending on the performance of the signal processor.

Ferromagnetic metal

  • The magnetic resistor section of the AMR sensor is a thin film of alloy consisting of nickel, iron, copper, and other substances, and this alloy is ferromagnetic metal.
  • In ferromagnetic metal, the electrical resistance changes based on an external magnetic field.
  • When ferromagnetic metals are subjected to an external magnetic field, at the molecular level, rotation in the 3d-band electron orbital plane occurs, and combined with the interaction of the inherent spin orbit of the electrons, this causes distortion in the 3d-band electron distribution (d-band wave function is distorted). As a result, the electrons seek energy stability, and this incites a change in the conduction electron probability of occurrence in the 4s-band, which is a different electron orbit, and this state is manifested as a change in electrical resistance.

G-H-I

Hoff

Hoff is the strength of the magnetic field when switching off the AMR sensor.
The figure in the datasheet shows the required magnetic field in order to switch off the AMR sensor at all times under fixed conditions.

Hon

Hon is the strength of the magnetic field when switching on the AMR sensor.
The figure in the datasheet shows the required magnetic field strength in order to switch on the AMR sensor at all times under fixed conditions.

Hysteresis

Hysteresis is the gap (setting span) between the magnetic flux density when the AMR sensor output turns on and when it turns off.
The AMR sensor was designed so that the magnetic flux density that occurs at a High output is shifted from the magnetic flux density at Low output, and this is used to prevent the occurrence of chattering in switching.
* This is not the difference between Hon and Hoff in the datasheet (example: 0.5 to 2.5mT for the MRMS501A-001).
(Although it varies depending on the individual product, the hysteresis is around 0.1 to 0.4mT. Typically, the size of the hysteresis is not specified in the specifications.)

ICs

  • ICs are circuits that perform digital processing on the same PCB as the elements.
  • Depending on the strength of the applied magnetic field, the output signal changes when the potential difference, which is changed by analog signals, exceeds a preset threshold value. Because the output is Hi or Lo only, signal processing is simple.

M-N-O

Magnetoresistance effect

In thin alloy films consisting primarily of nickel, iron, copper, and other ferromagnetic metals that are used in magnetoresistance elements, when the ferromagnetic metals are subjected to an external magnetic field, at the molecular level, rotation in the 3d-band electron orbital plane occurs, and combined with the interaction of the inherent spin orbit of the electrons, this causes distortion in the 3d-band electron distribution (d-band wave function is distorted).
As a result, the electrons seek energy stability, and this incites a change in the conduction electron probability of occurrence in the 4s-band, which is a different electron orbit, and this state is manifested as a change in electrical resistance.

mT

Millitesla. Name for unit of magnetic flux density. (SI units)
The conversion with the CGS unit of gauss is 1mT = 10 gauss.

Non-contact

  • Non-contact indicates that operations can be performed without direct contact.
  • For AMR sensors, boards with installed sensors are contained in the product, and this enables usage for the following applications.
    • Sensors that are not directly visible.
    • Switches that are easily adaptable into a waterproof structure
    • Switches that you do not want to reveal to the user
    Their properties allow an extremely wide range of applications, such as enabling operation from outside the sensor when the case is made of materials where magnetic forces pass through.
  • Locations that use reed switches have contacts, but AMR sensors do not have any contacts. In locations with harsh operating environments, such as those subjected to impacts or vibrations, AMR sensors can provide higher reliability. In some cases, the same magnet as the reed switch can be used without any modifications.

P-Q-R

Permalloy

Permalloy is a nickel-iron alloy. One characteristic of permalloy is that its resistance changes when subjected to a magnetic field from a certain direction. AMR sensors use this characteristic to function as magnetic switches.

Resistance value

  • AMR sensors use resistors that change based on the magnetic force.
  • Resistance values vary by the product, but they can range from several hundred Ω to several hundred kΩ. They change by up to 3% based on the size and direction of the magnetic force.
  • Whereas higher resistance values have the advantage of reducing the current consumption, they result in longer current paths, and so larger sizes are required for the element. Narrow elements can lead to process stability issues and the inability to obtain sufficient changes.
    Murata Manufacturing's AMR sensors exemplify our cutting-edge techniques for developing and providing sensors with compact sizes and low power consumption.

Response frequency (drive cycle)

This checks at a specific timing whether there is a magnetic field that can be turned on. This timing is called the drive cycle. A quicker drive cycle can be used in rotation detection and other applications, but it has a higher current consumption. A slower drive cycle enables a lower current consumption, and is used in open/close detection and similar applications.

S-T-U

Sensitivity

The sensitivity is the strength of the magnetic force that turns on (or off) the AMR sensor. The ON sensitivity (Hon) is the magnetic force that turns on the AMR sensor which was off with no or weak magnetic field, and the OFF sensitivity (Hoff) is the magnetic force that turns off the AMR sensor which was on with a strong magnetic field.

Temperature characteristics

AMR sensors contain permalloy (nickel-iron alloy), which is a material whose sensitivity varies based on the outside temperature. Generally, permalloys exhibit higher sensitivity at low temperatures and lower sensitivity at high temperatures.
Also, some AMR sensors include temperature compensation circuits that give the sensors lower sensitivity at low temperatures and higher sensitivity at high temperatures for canceling out the temperature characteristics of permalloys and reducing the variation in sensitivity for the sensor.

V-W-X

Variation in sensitivity

The AMR sensor sensitivity varies by individual AMR sensor. The Hon and Hoff in the datasheet indicate the specific range for that product.