What is a Thermistor?

- Basic Knowledge of Thermistors -

 


 Thermistor TOP
   
Basic Knowledge   Selection Guide  
Application Example  
Glossary  
Discontinued Products Information
Thermistors are electronic components in which the resistance changes with the change of temperature.
Thermistors are categorized into the following 2 types according to how the resistance changes.

NTC Thermistors


What is an NTC Thermistor? >

Function Temperature Characteristics Appearance / shape
The resistance drops as the temperature increases.
For temperature sensing, compensation and inrush current suppression.



 NTC Thermistor TOP >


PTC Thermistors


What is an PTC Thermistor? >

Function Temperature Characterristics Appearance / shape
The resistance remains constant up to a certain temperature, and  suddenly increases at a certain critical temperature.
For overheat sensing, overcurrent protection, inrush current suppression and heater.



 PTC Thermistor TOP >