Q&A: Murata’s recent innovations for Mobility
Q: What recent innovation has Murata Manufacturing Co Ltd introduced to meet the demands of the automotive industry?
A: Murata Manufacturing Co Ltd has recently launched the XRGE_M_F series of state-of-the-art electronic timing devices, specifically designed to meet the stringent performance requirements of automotive electronic systems, such as In-Vehicle Networks (IVN), wireless communication, and Advanced Driver Assistance Systems (ADAS).
These SMD type crystal units offer exceptional accuracy (±40ppm) and reliability, even in extreme temperature conditions ranging from -40°C to +125°C and can be used without tuning for wireless communication functions (BLE/Zigbee, etc) such as for automotive TPMS, RKE and BMS.
Q: Why is precise timing technology critical in addressing evolving trends in the automotive sector?
Current trends in the automotive industry such as increasing Electric Vehicle (EV) adoption, increasing levels of vehicle autonomy and the rise of the connected car are driving significant innovation in automotive electronics. The modern car is a complex, mobile system, which relies heavily on electronic subsystems to deliver critical functionality, including Advanced Driver Assistance Systems, (ADAS), motor control, braking systems, battery management, steering control, in-vehicle networking and many more. Arrays of sophisticated sensors collect information not only on the car itself, but also on its surrounding environment, generating terabytes of data every hour. In-vehicle networks enable this data to be accessed by the relevant onboard subsystems while increasing use of wireless networking enables V2X functionality, where the car can share data and communicate with other road users as well as with cloud-based services.
Timing technology is crucial to the operation of most digital systems, ensuring everything from the smooth transmission of data to communication between individual subsystems. Today’s cars use anywhere between 20 and 70 standalone timing devices, with this number growing as each new generation of car adopts increasingly advanced technology. Timing components synchronize critical clocking functions within ADAS, vehicle networking, infotainment and other subsystems and also facilitate communication between the subsystems and the various sensors.
In summary, the need for high accuracy and reliability in automotive timing devices is a response to the increasing complexity, safety requirements, and consumer demands in the automotive industry. Ensuring that these components can deliver precise performance under a wide range of conditions is essential for the development of current and future automotive technologies.
Q: How does the increasing complexity of automotive electronic systems drive the need for high-performance timing devices?
A: Multiple automotive systems need extremely robust timing references delivering constantly stable timing signals, even under environmental stressors like high temperature, rapid thermal changes, airflow, shock, vibration, and electrical noise.
ADAS and security systems employ a comprehensive array of networked sensors and technology to detect and warn of pedestrians, obstructions and blind spots, control steering, actively control braking and many more. High performance timing devices are critical to the operation of many of these sensors and are also essential for the synchronization and frequency stability of the internal operations of vehicle electronic control units (ECU).
Sensors such as proximity/collision sensors, light detection and ranging (LiDAR) systems, along with global positioning systems (GPS), diagnostic interfaces, and battery management systems (BMS) produce huge volumes of real-time data. Autonomous vehicle functionality requires critical decisions to be made on this data in real-time, and any lag or disruption to the processing of this data could have severe consequences. Designers are therefore increasingly relying on In-Vehicle Network technologies such as Controller Area Network (CAN) and Ethernet which rely on accurate timing to maintain their integrity.
Connected vehicles are increasingly sharing data with other road users and with cloud-based applications such as remote maintenance and traffic monitoring, leading to the integration of wireless technologies such as Bluetooth®, NFC, and Wi-Fi in vehicles. These wireless technologies require precise timing to manage communication protocols and ensure seamless connectivity.
Q: What are the design considerations for automotive engineers when selecting timing devices for modern vehicles?
A: Automotive designers face the twin challenges of adopting more complex solutions while improving system-level reliability. Automotive electronics must be capable of operating in hostile environments, where they are subject to constant vibration, shock, EMI interference and extreme temperature variations.
When selecting a timing device, the designer must be confident that it will deliver the ±40ppm frequency accuracy levels required by the various vehicle communication and safety functions. The device must be capable of withstanding the hostile automotive environment and must maintain its accuracy over the entire -40°C to +125° operating temperature range. Most importantly, integrating the device into the overall solution should require minimal design effort and cost.
Designers must also consider component lifecycle and availability when choosing the right timing device for their automotive solution. The selected device must not become obsolete during the lifecycle of the vehicle and the designer must be confident that multiple sourcing options exist, to guarantee its availability.
Q: What sets Murata's new timing device apart in terms of its specifications and benefits for automotive applications and what makes Murata's HCR technology unique compared to other timing solutions in the market?
A: Murata's high accuracy and high-temperature automotive crystal (HCR), or XRCGE_M_F series, is the first in the world to achieve a total frequency tolerance of ±40 ppm across an operating temperature range of -40°C to +125°C. This HCR device is unique due to its groundbreaking resin-sealed package technology and optimised crystal design, enabling high-temperature operation and high accuracy.
Previous generations of timing devices were unable to maintain required accuracy levels cross the full temperature range without the addition of tuning ICs. Devices also suffered from premature aging due to the hostile conditions of the automotive environment. The Murata XRGE_M_F crystal devices do not require correction by tuning ICs, contributing to a significant reduction in design man-hours and manufacturing costs, and also have improved aging characteristics.
The features of the XRCGE_M_F make it ideal for supporting the latest vehicle communication and safety functions, such as CAN and ethernet IVNs, ADAS components (cameras, LIDAR, RADAR), and wireless communication technologies (RF, NFC, BLE, ZigbeeTM, UWB).
Q: How does the evolution of automotive technology impact the design and deployment of electronic components like timing devices and how does Murata’s HCR device support future trends in autonomous driving and vehicle connectivity?
The automotive industry is moving towards greater integration and miniaturisation of electronic components to accommodate the increasing number of critical electronic systems in vehicles. These advancements necessitate components that can maintain accuracy without the need for system calibration or temperature compensation, especially as features like Bluetooth® Low Energy (BLE) and ethernet become standard in vehicles.
With its compatibility with automotive applications such as IVNs, ADAS, and wireless communication systems, its lifecycle durability and compliance with automotive regulations, the Murata XRCGE_M_F series are ideally placed to support current and future automotive solutions.
Q: How does Murata ensure the long-term reliability and availability of its HCR components for the automotive industry?
A: Through its unwavering commitment to maintaining component availability amidst global supply challenges, Murata ensures the reliability of the XRCGE_M_F series of HCR components through a stable and reliable multi-source supply chain. This approach addresses any potential supply concerns for automotive users, ensuring timely delivery for OEMs. Additionally, the high temperature operating window and strong resistance to solder cracks guarantee the long-term reliability of the components.