Building Reliable Wireless Vehicle Communication to Unlock the Future of Transportation

Meet our CEO
Figure 1 – Connected mobility is widely regarded as a vital component of the future of transportation (Source: Murata)

The integration of reliable wireless communication systems is essential for next-generation vehicles. The convergence of automotive technology and digital connectivity signals the start of a revolutionary era in transportation, offering improved safety, higher user satisfaction, and unmatched automation.

As intelligent vehicles advance, driven by sensor technology, AI, and data analytics, their ability to perceive surroundings, make real-time decisions, and communicate with other vehicles and infrastructure becomes paramount. Nonetheless, the journey towards achieving fully autonomous driving is accompanied by various hurdles, including the efficient exchange of data between vehicles and their environment. Hence, as automated vehicles become more prevalent, the significance of dependable wireless communication solutions intensifies.

The Push for Higher Autonomous Driving Levels
The U.S. Society of Automotive Engineers (SAE) outlines six levels of vehicle autonomy, from Level 0 (no automation) to Level 5 (full automation). Each level represents a step towards fully automated driving, with increasing demands on the vehicle's control and communication systems.

  • Level 0: No automation – the driver performs all tasks.
  • Level 1: Driver assistance – the system aids with sub-tasks.
  • Level 2: Partial automation – the system handles sub-tasks but requires human supervision.
  • Level 3: Conditional automation – the system manages all tasks in certain conditions but may need human intervention.
  • Level 4: High automation – the system is designed to be highly automated, requiring human intervention only in certain situations.
  • Level 5: Full automation – the system manages all tasks in all conditions.

As vehicles reach higher levels, particularly Level 3 and beyond, it becomes vital for them to communicate in real-time with centralized services and supporting infrastructure through Vehicle-to-Everything (V2X) technology. This is necessary to maintain both safety and efficiency and includes information such as their location and movements, ensuring safe distances and collision avoidance.

The Value of Vehicle-to-Everything (V2X) Communication
Achieving higher levels of autonomy brings new challenges. At the frontline, vehicles require a larger quantity of advanced sensors and controllers are needed to ensure spatial awareness and the capability to adjust to diverse scenarios, including unpredictable weather and road conditions.

But while vehicle systems are the core components for highly autonomous vehicles, behind the scenes, communication technologies also play a vital role in addressing unforeseen dangers. For example, while an advanced driver-assistance system (ADAS) can activate automatic braking to prevent a frontal collision, wireless communication can further enhance the safety of this function by notifying sequential cars behind to take similar action. Wireless communication has the ability to alleviate urban congestion and safety by enabling infrastructure to notify vehicles of forthcoming traffic and suggest alternate routes, as well as transmitting critical messages regarding changes in road speed or conditions.

But to achieve both autonomous operation and more sophisticated vehicle to infrastructure interactions, vehicles need advanced V2X communication, encompassing both vehicle-to-vehicle (V2V) and vehicle-to-infrastructure (V2I). This smart relationship between vehicle and infrastructure is known as the Intelligent Transport System (ITS) (Figure 2).

Figure 2 – A comparison between a conventional setup and the PoC method complete with Bias-T filter circuits (Source: Murata)

ITS encompasses V2I and V2V communication methods, along with other means of facilitating the exchange of crucial information among vehicles and their surroundings. mitigating potential dangers and increasing the efficiency of roads. In anticipation of such communication, nations are implementing specific standards to guarantee smooth V2X communication. For example, Japan uses ARIB STD-T109 (760 MHz band), while Europe and the U.S. have adopted IEEE 802.11.P (5.9 GHz band).

At the core of ITS vehicles are telematics control units (TCUs) which play a vital role in ensuring vehicle safety and operation. These units will rely on wireless, cellular, and satellite communication standards like 5G and Global Navigation Satellite Systems (GNSS). Through the amalgamation of these communication methods with TCUs and the essential assortment of vehicle sensors and control systems, vehicles will be able to accurately monitor and thus traverse in a three-dimensional space. Consequently, this will enable autonomous operation in remote rural areas with limited network coverage, as well as in complex urban environments plagued by noise and multipath errors.

Ensuring Reliable Communication
As vehicles evolve into the era of the ITS reliable wireless communication becomes critical for both operation and safety. High-quality communication requires a range of supporting passive components. Murata is committed to automotive reliability and offers a wide range of solutions that meet the AEC-Q200 standard for automobiles. This includes an extensive portfolio of products that are suitable for telematics control units (TCUs) (see Figure 3) as well as other critical areas of automotive communication.

Figure 3 – A block diagram showing an example of a TCU (Source: Murata)

Murata offers a comprehensive selection of components, such as inductors, capacitors, thermistors, and common mode choke coils (CMCCs). For Bluetooth and Wi-Fi communication, Murata recommends automotive-specific chip inductors from its LQW, LQP, and LQG series, known for their compact size, high performance, and reliability in harsh conditions.

Noise management is also crucial to ensuring effective communication systems. Murata's DLW32PH CMCCs for power lines excel in high-frequency noise suppression, essential for modern fast networks and vehicle electrification (Figure 4).

Figure 4 – The compact and highly robust DLW32PH (Source: Murata)

With its ability to substantially reduce noise, the DLW32PH is particularly beneficial in critical wireless automotive applications and is designed to guarantee communication integrity within the 200MHz-800MHz range.

Summary: Underpinning the Next Generation of Transportation
The future of transportation depends on the smooth integration of vehicles and infrastructure facilitated by dependable wireless communication systems. This fusion of automotive technology and digital connectivity heralds a new era, characterized by enhanced safety, user experience, and automation. However, the establishment of robust V2X communication is vital in order to address the obstacles of autonomous driving and facilitate seamless interaction between vehicles and their environment. High-quality passive components, like those from Murata, which have been tailored to the next generation of vehicles are essential for maintaining reliable communication, ensuring the success of intelligent connected vehicles and paving the way for a safer, more efficient driving environment.