Ceramic Capacitors FAQ

Characteristics

How do I use the function that compares the electrical characteristics of ceramic capacitors?

From the ceramic capacitor home page, search for products using one of the following search methods.

How do I use the function that compares the electrical characteristics of ceramic capacitors?

On the search results page, select the checkbox for the products you want to compare, and then press the Compare button (up to five part numbers can be selected).

The currently selected part numbers are remembered even if you leave the page. For example, you can compare two parts, A and B, by first searching for part number A and selecting it for comparison, and then searching for part number B and selecting it for comparison. Press the "Selected part numbers" button if you want to view or remove your selections.

If there is no electrical characteristic data associated with a part number, no checkbox appears and it cannot be selected.

How do I use the function that compares the electrical characteristics of ceramic capacitors?

The comparison graph results page shows the status, part numbers, and features of each part, indicating any differences in red. When you unselect a checkbox, it hides the graphs.

When you hover the cursor over the graph lines, the corresponding values are displayed. You can also print the graphs or download the values in CSV format.

How do I use the function that compares the electrical characteristics of ceramic capacitors?

You can press the "Setting details" button to change the type of graph or configure the axes.

How do I use the function that compares the electrical characteristics of ceramic capacitors?

For example, if you change the frequency characteristic lZl to Q on the graph and press the "Set using this content" button, the graph changes as follows.

How do I use the function that compares the electrical characteristics of ceramic capacitors?

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.
Send

For product inquiries, please contact us using our contact form.