Digital Panel Meters FAQQDo all of the above questions also apply to your DCA5-20PC series ammeters?

A
Yes, especially the question pertaining to ‘–DC1’ and ‘–DC4’ models. For application purposes, the primary difference between these two ammeter families is the location of the shunt resistor: DCA-20PC ammeters have an internal low-loss shunt connected across TB1, while DCA5-20PC ammeters work in conjunction with user-supplied, external 50mV or 100mV shunts connected to TB1.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.