LoRa FAQQWhy should I choose LoRa? Is LoRa(WAN) better than other technologies?

A

It is clear that LoRa is de facto dominant in a few (mainly European for now) markets in the public IoT network space. LoRaWAN has the benefit of being an alliance with an Open approach instead of a proprietary one. There are also technological differences between the various solutions.

However, the main question is and remains: What goals do you want to achieve with your IoT project?

No technology is perfect. The openness of LoRa is a benefit compared with the proprietary approach of Sigfox but, along with its reliance on unlicense spectrum this openness is also a problem.

There is never a one-size-fits-all solution. It is rarely about 'this' versus 'that' technology. In most cases it is about 'which mix of technologies will make me reach my IoT projects goals?'.

*Extracted from: LoRa and LoRaWAN: the technologies, ecosystems, use cases and marketOpen in New Window

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.