LoRa Module FAQ

Hardware

We are defining the antenna for our prototypes. Does the RF pin already have the matching components to have 50 ohm impedance, or we need to add it externally?

Please refer to my Murata.
We have the detailed information on the schematics, etc. The Pin is 50 ohms, but, there can be antenna tuning network which customer might implement. There is also reference antenna information that customer should use.

Return to LoRa Module Page

Back to LoRa FAQ List