LoRa Module FAQ

Software

What is the physical interface on device to load firmware (first time)? Is it possible to flash firmware through PIN 23 and 24? Do we need to connect to other PINS?

When customers load our modem firmware to TypeABZ-078 for the first time, we recommend them to use SW interface with ST-Link.

Return to LoRa Module Page

Back to LoRa FAQ List