Acceleration Sensors FAQ

Mounting

I would like to get some package information of your products on a component level. Is there a lid over the top or is the part filled with solid material? If there is a void (air or gas) inside how large is it?

Package of the Murata Electronics Oy's component is one-piece molded plastic package. There is a lid over the top and the volume of the gas cavity is approximately 20 mm3 in SCA 61T and app. 70 mm3 in SCA100T. In our stand-alone SCA125T module the cavity is app. 3,000 mm3.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.
Send

For product inquiries, please contact us using our contact form.