Inclinometers FAQQWhen using the SPI to communicate with the inclinometer, what is the maximum sampling rate?

A
The maximum practical sampling rate is approximately 500 Hz.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.