Infrared Sensors FAQ

Mounting

How we can do soldering for a Pyroelectric infrared sensor?

The soldering conditions for them are as follow. 
<LEAD Type>
Please perform the soldering of the terminal with an iron point solder.
Please mount the soldering of the terminal as quick as possible. Specifically, please go in the range of follows.
 •Iron point temperature:350゚C max.
 •Time:
  Terminal length from stem 1 to 3mm : Less than 3.0 sec by terminal.
  Terminal length from stem Over 3mm : Less than 10 sec by terminal.

<SMD Type>
The SMD type can be soldered with reflow soldering.

Both types can not be soldered with flow soldering(wave soldering).

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.
Send

For product inquiries, please contact us using our contact form.