Infrared Sensors FAQQCan we use Pyroelectric infrared sensor outside?

A
Yes, they can be used outside.
However, when the sensor is used outside, since there are many factors which generate a thermal change, it is more difficult to use the sensor outside than inside.
When sunlight and wind directly contact the sensor, an output may occur by reacting to the change in temperature caused by such factors.
Install the sensor in a location where there is no direct contact from sunlight and wind, and where there is no condensation.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.