Ultrasonic Sensors FAQ

Characteristics
Waterproof type/Open-Structure type/High-Frequency type

Is it possible to detect an object that is placed behind a film?

It depends on the thickness of the film and the distance to the object. It may be possible if the film is thin enough for the ultrasonic wave to penetrate and the object is placed at a short distance. 

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.
Send

For product inquiries, please contact us using our contact form.